Skip to main content
Associate III
April 8, 2024
Question

LIS2DW12 - Changing FIFO mode from bypass to cont-to-fifo

  • April 8, 2024
  • 2 replies
  • 1469 views

Greetings

I am running an application where I am using the LIS2DW12 accelerometer. I am using it for classical sampling of acceleration values in cont-to-fifo mode, which works fine. The FIFO is configured with the High pass filter enabled. 

I now want an additional 10 samples (preferably more than 4 samples but 10 being the max) with the high pass filter disabled. I have tried running the LIS2DW12 in single-sampling mode 10 times, with the following config:

 

 

-WriteReg(CTRL6, 2G full scale, ODR/2, LOW Noise enabled, HPF disabled)
-WriteReg(Fifo_ctrl, bypass)
-WriteReg(CTRL3, I2C_Single data conversion enabled)
-WriteReg(CTRL3, Start single data conversion)
while(DRDY bit is not set)
{
 Readreg(status)
}

- Read data registers(x, y, z)

-WriteReg(CTRL6, 2G full scale, ODR/2, LOW Noise disabled, HPF enabled)
-WriteReg(Fifo_ctrl, bypass mode)
-WriteReg(Fifo_ctrl, cont-to-fifo mode)
-WriteReg(CTRL3, Latched interrupts enabled)

 

 Once the above code runs in the loop and I provide a disturbance to the sensor for it to wake up and sample, the application stops responding.

Is there something I am missing, to disable and re-enable the FIFO to run properly?

 

 

This topic has been closed for replies.

2 replies

Federica Bossi
ST Technical Moderator
April 9, 2024

Hi @ZAIDS-S23 ,

The steps you need to follow to pass from bypass to continuous to FIFO mode are:

  • Configure the desired interrupt generator
  • Activate continuous-to-FIFO mode by setting the FMode[2:0] field to 011 in the FIFO_CTRL register (2Eh).
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ZAIDS-S23Author
Associate III
April 9, 2024

Hi Federica

I am familiar with placing the accelerometer in any FIFO mode of my choice and configuring it further in terms of interrupts etc.

However, what I am unsure of, is configuring it in bypass mode AFTER I've received an interrupt and read out the FIFO. After I read out the FIFO, I want to place it in single-data conversion mode and place the FIFO in bypass mode. 

From the steps I've implemented above, it doesn't seem to work consistently i.e. I can actually complete the above process uptil the point of placing it in bypass mode and then reading out 3 samples. But to do it repetitively, it cannot happen consistently. The chip stops responding to interrupts eventually.