Skip to main content
Visitor II
April 2, 2024
Question

LIS2DUXS12 Qvar and Interrupts

Hi all,

I am trying to implement the  LIS2DUXS12 into a design and I am wondering if it is possible to still use the interrupts while using the Qvar sensors. Ideally, I need a way to detect when the device is on the human body and also a way to wake up MCU when motion is detected. It appears this isnt possible with the Qvar leads taking up the interrupt lines.

Will this be possible with this device?

 

Thanks

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
April 10, 2024

Hi @Eyurk ,

Welcome to ST Community!

Yes it is possible. You find all the details on datasheet at page 17:

FedericaBossi_0-1712751335219.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.