Skip to main content
JWick.1
Associate
Jul 11, 2020 10:23 PM UTC
Solved

LIS2DH12 - Read (latched) INT2-activity via I2C for Motion Detection

Hello Team ST, Sensor: LIS2DH12

our application needs to detect motion activity. Since it is not time critical, we want to check this by reading the (latched) activity of INT2.

I can see the motion activirty on the INT2-pin, but I can NEVER see it on INT2_RRC (35h).

(CTRL_REG5 (24h)LIR_INT2 is set and CTRL_REG6(25h). I2_ACT and I2_IA2 too)

I have checked the datasheet and aAN5005 very carfully, but I have no idea what is wrong.

Thanks in advance for your help!

Juergen

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Jul 16, 2020 11:03 AM UTC

Hi Juergen, but are you maybe enabling the motion activity interrupt as a "software interrupt 1", but you want to drive this interrupt on INT2 physical pad? If so, you should check a pseudocode similar to the below one:

Write 20h into CTRL_REG3 // Interrupt activity 1 driven to INT2 pad
Write 00h into CTRL_REG4 // FS = ±2 g
Write 02h into CTRL_REG5 // Interrupt 2 pin latched
Write 10h into INT2_THS // Threshold = 250 mg
Write 00h into INT2_DURATION // Duration = 0
Write 0Ah into INT1_CFG // Enable XH and YH interrupt generation
Poll INT2 pad; if INT2=0 then go to 8 // Poll DRDY/INT2 pin waiting for the // wake-up event
Read INT2_SRC // Return the event that has triggered the interrupt
(Wake-up event has occurred; insert your code here) // Event handling

Regards

2 replies

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Jul 16, 2020 11:03 AM UTC

Hi Juergen, but are you maybe enabling the motion activity interrupt as a "software interrupt 1", but you want to drive this interrupt on INT2 physical pad? If so, you should check a pseudocode similar to the below one:

Write 20h into CTRL_REG3 // Interrupt activity 1 driven to INT2 pad
Write 00h into CTRL_REG4 // FS = ±2 g
Write 02h into CTRL_REG5 // Interrupt 2 pin latched
Write 10h into INT2_THS // Threshold = 250 mg
Write 00h into INT2_DURATION // Duration = 0
Write 0Ah into INT1_CFG // Enable XH and YH interrupt generation
Poll INT2 pad; if INT2=0 then go to 8 // Poll DRDY/INT2 pin waiting for the // wake-up event
Read INT2_SRC // Return the event that has triggered the interrupt
(Wake-up event has occurred; insert your code here) // Event handling

Regards

JWick.1
JWick.1Author
Associate
Jul 16, 2020 2:44 PM UTC

Hello Elon,

thank you very much for your reply! Yes, that seems to work. I can see the IRQs in the _SRC-register now.

I think the Accelerometer is used in many applications this way, maybe a few hints in the datasheet would be helpful for many users.

Best regards,

Juergen