Solved
LIS2DE12 Tolerance
I am using a LIS2DE12 to detect when a mechanical shock occurs to my device. The datasheet provides only nominal values for the sample rate and the sensitivity.
- What is the tolerance on the sample frequency, I am using the ODR nominal rate of 5376 Hz?
- What is the tolerance on the sensitive, I am using the +/-16 g range, which has a typical sensitivity of 187.5 mg/digit.
- What is the worst case temperature sensitivity?
- What is the worst case offset?
If worst case values are not available is there some characterization data which could provide some guidance?
Thank you.