Skip to main content
WSpar.1
Associate III
February 22, 2024
Question

lis2de12 landscape/portrait interrupt

I have this MEMS sensor on a custom board to detect landscape or portrait mode of my device.
The problem is that it doesn't generate an interrupt.

- 4D mode should be sufficient.
- Range 2g
- Tested different ODR settings.

 

My current code is now:

 

 

 

 

 

void tilt_init(void)
{

	dev_ctx.write_reg = platform_write;
	dev_ctx.read_reg = platform_read;
	dev_ctx.handle = &SENSOR_BUS;

	lis2de12_boot_set(&dev_ctx, PROPERTY_ENABLE);

	lis2de12_pin_sdo_sa0_mode_set(&dev_ctx, LIS2DE12_PULL_UP_DISCONNECT);
	lis2de12_high_pass_mode_set(&dev_ctx, LIS2DE12_NORMAL);

	lis2de12_device_id_get(&dev_ctx, &whoamI);

	/*Set Output Data Rate */
	lis2de12_data_rate_set(&dev_ctx, LIS2DE12_ODR_400Hz );

	/*Set full scale */
	lis2de12_full_scale_set(&dev_ctx, LIS2DE12_2g);

	/* Enable Block Data Update */
	lis2de12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);

	/*Configure power mode */
	//lis2de12_power_mode_set(&dev_ctx, IIS2DLPC_CONT_LOW_PWR_LOW_NOISE_12bit);

	/* Apply high-pass digital filter on Wake-Up function
	 * Duration time is set to zero so Wake-Up interrupt signal
	 * is generated for each X,Y,Z filtered data exceeding the
	 * configured threshold
	 */
	lis2de12_int1_gen_duration_set(&dev_ctx, 1);

	/*LPF2 on 6D function selection. */
	//lis2de12_6d_feed_data_set(&dev_ctx, IIS2DLPC_LPF2_FEED);

	/*Enable interrupt generation 6D & double tab on INT1 pin. */
	//lis2de12_pin_int1_route_get(&dev_ctx, &int_route.ctrl4_int1_pad_ctrl);

	lis2de12_int1_cfg_t lis2de12_int1_cfg = {0};
	lis2de12_int1_cfg._6d = PROPERTY_ENABLE;
	lis2de12_int1_cfg.xhie = PROPERTY_ENABLE;
	lis2de12_int1_cfg.xlie = PROPERTY_ENABLE;
	lis2de12_int1_cfg.yhie = PROPERTY_ENABLE;
	lis2de12_int1_cfg.ylie = PROPERTY_ENABLE;

	lis2de12_int1_gen_conf_set(&dev_ctx, &lis2de12_int1_cfg);

	lis2de12_int1_pin_detect_4d_set(&dev_ctx, PROPERTY_ENABLE);


	lis2de12_ctrl_reg3_t lis2de12_ctrl_reg3 = {0};
	lis2de12_ctrl_reg3.i1_ia1 = PROPERTY_ENABLE;

	lis2de12_pin_int1_config_set(&dev_ctx, &lis2de12_ctrl_reg3);

	//Set temp measuring
	lis2de12_temperature_meas_set(&dev_ctx, LIS2DE12_TEMP_ENABLE);

	/*
	 * Latched interrupt
	 */
	//iis2dlpc_int_notification_set(&dev_ctx, IIS2DLPC_INT_LATCHED);

}

 

 

 

 

 

 

Am I missing something crucial?

UPDATE:

Auch!, apparently the tilt interrupt pin number matched this wrong OR operation of other interrupt pins
Of all the pins you can choose as a designer!

Capture545454594.PNG

Still wondering how Tilt pin 0x0020 validates as true for if(GPIO == 0x4000 || 0x2000) 

Although this fixed the problem of handling interrupts correctly, it is still not generated bij the MEMS.
I only tested the interrupt pin manually

 

How can I setup the portrait/landscape threshold angle and rigger an interrupt?

This topic has been closed for replies.

2 replies

Federica Bossi
ST Technical Moderator
February 26, 2024

Hi @WSpar.1 ,

Have you already look at our PID examples on github?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate III
February 26, 2024

you mean 

 if(GPIO == 0x4000 || 0x2000) 

or

 if((GPIO == 0x4000) || (GPIO == 0x2000)) ?