Skip to main content
spa23
Associate III
August 30, 2021
Solved

LIS2DE12 interrup on wakeup

I have a simple task, to wake up the CPU when the device is shaken.

It should be pretty simple, the MEMS sensor samples with 10Hz until I shake it, then it samples with 100Hz, but I get no interrupt. :(

I use the driver form GIT hub and Interrupt INT1

https://github.com/STMicroelectronics/lis2de12/tree/21b9d1a565882a242143453580efb6abcd450686

My CODE:

/* Set full scale to 2g */

lis2de12_full_scale_set(&(phandler->ctx), LIS2DE12_2g);

/* route HP filter output on outputs registers */

lis2de12_high_pass_on_outputs_set(&(phandler->ctx), PROPERTY_ENABLE);

/* route HP filter output on interrupt generator 1 */

lis2de12_high_pass_int_conf_set(&(phandler->ctx), LIS2DE12_ON_INT1_INT2_GEN);

/* HP filter mode is "autoreset on inteerupt event" */

lis2de12_high_pass_mode_set(&(phandler->ctx), LIS2DE12_NORMAL_WITH_RST);

/* Set HP filter on mode */

lis2de12_high_pass_bandwidth_set(&(phandler->ctx), LIS2DE12_AGGRESSIVE);

/* Configure interrupt on threshold on x,y,z axis low / high events */

lis2de12_int1_cfg_t lis2de12_int1_cfg = {0};

lis2de12_int1_cfg.xhie = PROPERTY_ENABLE;

lis2de12_int1_cfg.yhie = PROPERTY_ENABLE;

lis2de12_int1_cfg.zhie = PROPERTY_ENABLE;

lis2de12_int1_gen_conf_set(&(phandler->ctx), &lis2de12_int1_cfg);

lis2de12_ctrl_reg3_t lis2de12_ctrl_reg3 = {0};

lis2de12_ctrl_reg3.i1_ia1 = PROPERTY_ENABLE;

lis2de12_ctrl_reg3.i1_ia2 = PROPERTY_ENABLE;

lis2de12_pin_int1_config_set(&(phandler->ctx), &lis2de12_ctrl_reg3);

lis2de12_lir_int1_t lis2de12_lir_int1;

lis2de12_lir_int1 = LIS2DE12_INT1_LATCHED;

lis2de12_int1_pin_notification_mode_set(&(phandler->ctx),lis2de12_lir_int1);

/* Set interrupt threshold at ~160 mg -> 1bit = 16mg@2g */

lis2de12_int1_gen_threshold_set(&(phandler->ctx), 10);

/* Set duration to zero - 1 bit = 1/ODR */

lis2de12_int1_gen_duration_set(&(phandler->ctx), 2);

/* Set Output Data Rate to 100Hz */

lis2de12_data_rate_set(&(phandler->ctx), LIS2DE12_ODR_100Hz);

lis2de12_act_threshold_set(&(phandler->ctx), (1000/16));

lis2de12_act_timeout_set(&(phandler->ctx), 10);

hope there is someone who can give a hint.

This topic has been closed for replies.
DSull.3
DSull.3Best answer
Visitor II
August 30, 2021

Hi, searching in the github examples, various examples implementing wake-up feature set duration of the event equal to 0 (I see you are setting 2):

/* Apply high-pass digital filter on Wake-Up function
 * Duration time is set to zero so Wake-Up interrupt signal
 * is generated for each X,Y,Z filtered data exceeding the
 * configured threshold
 */
 lis2ds12_wkup_dur_set(&dev_ctx, 0);

Moreover, they set a lower Interrupt threshold, typ 02h.

https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2ds12_STdC/examples/lis2ds12_wake_up.c

Did you check other interrupts as for example the data ready I1_ZYXDA one?

\Dk

2 replies

DSull.3
DSull.3Best answer
Visitor II
August 30, 2021

Hi, searching in the github examples, various examples implementing wake-up feature set duration of the event equal to 0 (I see you are setting 2):

/* Apply high-pass digital filter on Wake-Up function
 * Duration time is set to zero so Wake-Up interrupt signal
 * is generated for each X,Y,Z filtered data exceeding the
 * configured threshold
 */
 lis2ds12_wkup_dur_set(&dev_ctx, 0);

Moreover, they set a lower Interrupt threshold, typ 02h.

https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2ds12_STdC/examples/lis2ds12_wake_up.c

Did you check other interrupts as for example the data ready I1_ZYXDA one?

\Dk

spa23
spa23Author
Associate III
August 30, 2021

setting the duration  to 0 dit the work!

Thanks, you the best..