Skip to main content
GRose.2
Visitor II
December 7, 2020
Question

LIS2DE12 current draw

I am using a LIS2DE12 however I can't get the current on the VDD_IO to drop below 25uA.

Is there any reason for this?

My current settings are:

CTRL_REG1 = 0x3F

CTRL_REG2 = 0x30

CTRL_REG3 = 0x40

INT1_CFG = 0x0A

INT1_THS = 0x25

I am running off a 3V supply.

Cheers,

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
December 9, 2020

Hi @GRose.2​ ,

Are the Vdd and Vdd_IO supply lines separated? And, if so, are you measuring the current separately on both of them?

Moreover, are you running data acquisition during the current measurement? If yes, using SPI or I2C?

If so, the consumption on the Vdd_IO line is reasonable, since you are commuting the output voltage. And especially if you are using the I2C protocol, you will have a consumption due to the current flow through the pull-up resistors.

If you are not acquiring the output, which is the SDO/SA0 configuration in your application?

-Eleon