Skip to main content
Associate III
Nov 7, 2025 3:54 PM UTC
Solved

Linux device tree and IIO drivers for LIS2DW12 and IIS2DLPC, software compatiblity?

Greetings,

I am bring up a new HW design with the IIS2DLPC accelerometer integrated into the design.

I am trying to bring up a Linux IIO device driver for this device, and the kernel does not currently have 

direct support for the IIS2DLPC, however it does support the LIS2DW12, which from looking at the

datasheet for both, they appear to be SW compatible.

Can I just code the device tree node to specify the LIS2DW12?

accelerometer@18 {

compatible = "st,lis2dw12";
reg = <0x18>;
status = "okay";
st,drdy-int-pin = <1>;
interrupt-parent = <&sysfpga>;
interrupts = <SYSFPGA_INT_ACCELEROMETER>;
interrupt-names = "ACCELEROMETER-INT1";
};

Thanks,

Ken

 

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Dec 24, 2025 9:43 AM UTC

Hi @microcoder ,

Yes, IIS2DLPC and LIS2DW12 are similar.

You can start with the LIS2DW12 driver as a base but should thoroughly test and be ready to adapt the driver. For full support, developing a dedicated IIS2DLPC driver is recommended.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Dec 24, 2025 9:43 AM UTC

Hi @microcoder ,

Yes, IIS2DLPC and LIS2DW12 are similar.

You can start with the LIS2DW12 driver as a base but should thoroughly test and be ready to adapt the driver. For full support, developing a dedicated IIS2DLPC driver is recommended.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate III
Dec 24, 2025 3:51 PM UTC

Thank you!