Skip to main content
MBoch.2
Associate II
September 18, 2023
Solved

li2dw12, Does the "LP_MODE" value make effect, if high performance is set in the "MODE" of CTR1

We have following configuration in CTRL1: 

ODR[3:0]: 1001b (High-Performance / Low-Power mode 1600/200 Hz)

MODE[1:0]: 01b(High-Performance Mode (14-bit resolution))

And the value in the  "LP_MODE[1:0] " might be different depending on the state we came from. 

The question here does the value in the "LP_MODE[1:0] " have any affect in this configuration when high performance is selected in MODE[1:0]?

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
September 18, 2023

Hi @MBoch.2 ,

If you select High performance Mode with the bits MODE [1:0] than leave the LP_MODE[1:0] at the default value so that the high performance configuration will not be affected.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster :)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
September 18, 2023

Hi @MBoch.2 ,

If you select High performance Mode with the bits MODE [1:0] than leave the LP_MODE[1:0] at the default value so that the high performance configuration will not be affected.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster :)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.