Skip to main content
Evelina CAMILLERI
ST Employee
Jul 15, 2021 8:29 AM UTC
Solved

Large part of development goes into the data gathering/preparation and model creation. How is the model protected once it is on the ISM330DHCX from prying eyes?

..

    This topic has been closed for replies.
    Evelina CAMILLERI
    ST Employee
    Jul 15, 2021 8:29 AM UTC

    The decision tree needs to be uploaded in the sensor at every turn-on cycle from MCU side. This means that, if somebody can sniff the communication bus, can also get in possession of the required register writings to implement the decision tree. Also, the decision tree is uploaded in the sensor RAM without any encryption and can theoretically be downloaded. However, it can be from tricky to impossible to somebody that gets in possession of the RAM content/register writings to adapt the decision tree to its application, since ST does not provide any information on how to interpret the register/RAM content.

    1 reply

    Evelina CAMILLERI
    Evelina CAMILLERIAuthorBest answer
    ST Employee
    Jul 15, 2021 8:29 AM UTC

    The decision tree needs to be uploaded in the sensor at every turn-on cycle from MCU side. This means that, if somebody can sniff the communication bus, can also get in possession of the required register writings to implement the decision tree. Also, the decision tree is uploaded in the sensor RAM without any encryption and can theoretically be downloaded. However, it can be from tricky to impossible to somebody that gets in possession of the RAM content/register writings to adapt the decision tree to its application, since ST does not provide any information on how to interpret the register/RAM content.