Skip to main content
raffaelemariotti
Visitor II
February 11, 2014
Question

L3G4200D SPI communication problem

Posted on February 11, 2014 at 22:11

Hi all,I'm trying to read data from a L3G4200D gyro through an SPI module of aPIC32MX460F.The following is the code I'm using:

void

Spi1STL3G4200DConfig(

void

) {

unsigned

int

configA, configB;

int

rData;

configA = SPI_MODE8_ON |

SPI_CKE_ON |

CLK_POL_ACTIVE_HIGH |

MASTER_ENABLE_ON |

SEC_PRESCAL_3_1 |

PRI_PRESCAL_4_1;

// 80/12 = 6.66Mhz

configB = SPI_ENABLE;

rData = SPI1BUF;

IFS0CLR = 0x03800000;

SPI1STATCLR = 0x40;

OpenSPI1(configA, configB);

//configuro i pin SPI1

mPORTDSetPinsDigitalOut(BIT_0 | BIT_9 | BIT_10);

mPORTCSetPinsDigitalIn(BIT_4);

//C4 input digitale

if

(STL3G4200D_SpiReadRegister(WHO_AM_I) != 0xD3)

// ALWAYS OK !

return

-1; DelayMs(200);

STL3G4200D_SpiWriteRegister(CTRL_REG1, 0b00001111);

STL3G4200D_SpiWriteRegister(CTRL_REG5, 0b00000010);

//low pass filtering

DelayMs(200);

STL3G4200D_SpiReadRegister(0x29);

// ALWAYS FAILS WITH CODE HANGING AT SECOND ''while (!SPI1STATbits.SPIRBF)''

}

int

STL3G4200D_SpiReadRegister(

char

address){

int

toRead;

address |= 0x80;

//stiamo leggendo....0xA9 dopo l'OR

CS1GYRO = 0;

// _RD9

SPI1BUF = address;

while

(!SPI1STATbits.SPIRBF);

toRead = SPI1BUF;

// ALWAYS 0xFF AFTER GYRO INIT

SPI1BUF = 0x00;

while

(!SPI1STATbits.SPIRBF);

// CODE HANGS HERE AFTER GYRO INIT

toRead = SPI1BUF;

CS1GYRO = 1;

return

toRead;

}

void

STL3G4200D_SpiWriteRegister(unsigned

int

address, unsigned

int

data) {

address &= 0x7F;

//vogliamo scrivere

CS1GYRO = 0;

SPI1BUF = address;

//SPI.transfer(address);

while

(!SPI1STATbits.SPIRBF);

SPI1BUF = data;

//SPI.transfer(data);

while

(!SPI1STATbits.SPIRBF);

CS1GYRO = 1;

}

The code always hangs after gyro initialization and after the successful reading ofdevice ID.I use the same code

(with different prescaler values according to therequested SPI clock rates) to read XYZ channels from accelerometerswithout any problem. Lastly I'm able to read data from the gyro using I2C communicationprotocol but I needperformance so I'd like to use SPI module.Thank's for your help.Raffaele

This topic has been closed for replies.