Skip to main content
KShet.1
Associate
June 6, 2022
Solved

Issue with running X-CUBE-MEMSMIC1 (version 5.6.0), UltrasoundFFT on STEVAL-STWINKT1

Hello, 

I am able to successfully compile X-CUBE-MEMSMIC1 (version 5.6.0), UltrasoundFFT for STM32L4R9ZI-STWIN (STEVAL-STWINKT1) - as Debug .bin file. 

However, when I run it on the STWINKT1, the host Utility/GUI (UltrasoundFFT.exe) does not run. It is unresponsive when click the START button. Basically, the utility program hangs.

Alternatively, I don't have this problem when I use the compiled code from X-CUBE-MEMSMIC1 (version 5.5.0). It works fine.

I am wondering if anyone has tested this project (UltrasoundFFT for STWINKT1) using version 5.6.0? The Release Notes for version 5.6.0 says that "now using new GenericFFT library". I am wondering if there is any bug in this library (GenericFFTLibrary) versus the previous one used in version 5.5.0.

( I am using STM32CubeIDE version 1.9.0 on MS Windows 10, x64 PC for compiling.)

Thanks for any suggestion,

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
June 13, 2022

Hi @KShet.1​ ,

after internal checking with our experts, yes, you are right, the Ultrasound FFT demo for STWIN has a few (known) bugs.

A maintenance release of the X-CUBE-MEMSMIC1 firmware package is scheduled for end July: this release will include the solution of this bug.

Please check the X-CUBE-MEMSMIC1 page in some weeks --> X-CUBE-MEMSMIC1.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
June 13, 2022

Hi @KShet.1​ ,

after internal checking with our experts, yes, you are right, the Ultrasound FFT demo for STWIN has a few (known) bugs.

A maintenance release of the X-CUBE-MEMSMIC1 firmware package is scheduled for end July: this release will include the solution of this bug.

Please check the X-CUBE-MEMSMIC1 page in some weeks --> X-CUBE-MEMSMIC1.

-Eleon