Hello @DLlam.1 and welcome to the Community :)
The X-NUCLEO-IKS01A3 is compatible with Nucleo-L552ZE-Q (with STM32 Nucleo boards)
Maybe you have to check solder bridges.
You can check if the available -ready to use- examples with STM32L5 are working.
Make sure to include the IKS01A3 from the BSP folder under X-CUBE-MEMS package:
STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\8.3.0\Drivers\BSP
and Import the Components folder from X-CUBE-MEMS package: STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\9.2.0\Drivers\BSP\Components
then, add it in the Components folder of the CubeL5 package:
STM32Cube\Repository\STM32Cube_FW_L5_V1.4.0\Drivers\BSP\Components
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks