Skip to main content
Associate
Sep 15, 2026 9:42 AM UTC
Solved

ISM6HG256X / Shock event

Hi, 

 

we use on a design a ISM6HG256X. We want to detect a shock end event using the interrupt INT2.

We use this configuration :

    * INT2_HG_WU = 0

    * INT1_HG_WU = 0

    * INT2_HG_SHOCK_CHANGE = 1 

    * INT1_HG_SHOCK_CHANGE = 0

Logically, we should have an interrupt INT2 only when the shock event end is detected. In fact, we have an interrupt at wake_up event and at the shock end and sometimes we have interrupt on INT1. 

We use a STEVAL - MKI248KA to evaluate the ISM6.

Do you have some tips to solve this problem?

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 15, 2026 3:12 PM UTC

Hi ​@David45 ,

When the high-g accelerometer is enabled, the low-g accelerometer cannot stay in power-down. It must run in High-Performance or High-Accuracy ODR mode. However, the low-g and high-g ODRs are independent and can be configured separately.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

Federica Bossi
ST Technical Moderator
Sep 18, 2026 6:53 AM UTC

Hi ​@David45 ,

On ISM6HG256X, the high-g wake-up and shock interrupts are ORed, so a shock event is not reported as a “pure” end-of-shock signal only. To identify the exact phase, read ALL_INT_SRC first and then HG_WAKE_UP_SRC, and check HG_SHOCK_STATE / HG_SHOCK_CHANGE_IA to distinguish wake-up, shock entry, and shock end.
Also make sure no other sources are routed to INT1/INT2, because multiple interrupt sources are combined with an OR logic on the same pin.
Finally, when the high-g function is enabled, the low-g accelerometer must be in high-performance or high-accuracy ODR mode; low-power, normal, and ODR-triggered modes are not compatible.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
David45Author
Associate
Sep 18, 2026 1:00 PM UTC

Hi Frederica, 

 

Thanks for your answer. We will check the INT sources in case where we forget one sources. 

Just a question about low g, we need to be in high performance in our case but the low g could stay in power down or it must run all the time we use the High g ?

 

 

 

 

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 15, 2026 3:12 PM UTC

Hi ​@David45 ,

When the high-g accelerometer is enabled, the low-g accelerometer cannot stay in power-down. It must run in High-Performance or High-Accuracy ODR mode. However, the low-g and high-g ODRs are independent and can be configured separately.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.