Skip to main content
GnR
Associate II
August 9, 2022
Question

ISM330DLC CS and OCS_Aux pin states

If the ISM330DLC is connected to two separate dedicated SPI buses (i.e. no other SPI slaves on the bus) can the CS and OCS_Aux pins be connected to ground or do they have to be controlled by their respective SPI masters?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    August 12, 2022

    Hi @GnR​ ,

    let me check if I well understood the question. You have an ISM330DLC wired to two different SPI lines (so basically these lines are shorting at the device pad level): if so, you cannot set one of the two (or both) CS to GND, since you need them to be driven low or high for starting and ending the SPI communication.

    For the OCS_Aux pin, as stated in the datasheet, if you don't need it you have to left it unconnected (Leave pin electrically unconnected and soldered to PCB).

    -Eleon