Skip to main content
Visitor II
Aug 3, 2026 11:10 AM UTC
Question

ISM330DHCX Self-test failed

Hello,

The self-test for the ISM330DHCX failed.
What could be the cause?

I performed the self-test following the procedure in application note AN5398.
The test failed (NG) on the negative side of the Z-axis for the gyroscope function.
When measuring the I2C waveforms, the data output by the IC at registers 26h and 27h showed values ​​consistent with a self-test failure.

Incidentally, I am turning to this community because the distributor's support has been poor.

Regards,

 

 


Japanese memo
こんにちは

ISM330DHCXのセルフテストに失敗した。
原因は何が考えられるか?

アプリケーションノートAN5398の手順に沿ってセルフテストを行った。
ジャイロセンサ機能のZ軸のネガティブでNGが出た。
I2C波形を測定するとICが出力しているデータ26h、27hのデータがセルフテストNGになるような数値を出力している。


ちなみに商社の対応が悪いからこのコミュニティを頼っている。

1 reply

Federica Bossi
ST Technical Moderator
Aug 25, 2026 8:49 AM UTC

Hi ​@洋平_it ,

How many parts are failing?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.