Skip to main content
Visitor
Nov 18, 2026 3:09 PM UTC
Question

ISM330DHCX + IIS2MDC on one I2C bus - schematic check (Mode 1 pins, IIS2MDC C1 and INT/DRDY)

We are developing the CoCaptain Bosun, a battery-powered marine tracker and anchor alarm for sailing yachts (ESP32-S3, LTE Cat-1 modem, dual-band GNSS, 1S Li-ion with BQ25895 charger, boat supply 9-32 V). Prototype run of 5-10 boards at JLCPCB, 4 layers, 90 x 70 mm. The schematic was drawn in KiCad 10; sheet titles and some comments are in German.

The attached sheet shows the ISM330DHCX (U17) and the IIS2MDC (U18) on the shared I2C bus (3.3 V).

  1. ISM330DHCX in Mode 1, SDx and SCx tied together to GND via 10 kΩ. Is a common resistor acceptable?
  2. IIS2MDC: C1 = 220 nF, about 1.3 mm from pins 5/6. Is this close enough? INT/DRDY is not used and tied to GND through 100 kΩ (forum reports of high idle current with the pin floating). Is a pull-down the right choice, or should it be left open with the interrupt disabled?

Thank you very much for your time.

Best regards,
Robert Fraefel
CoCaptain (cocaptain.ch)