Skip to main content
Associate
Jan 27, 2025 7:45 PM UTC
Solved

ISM330 how is INTERNAL_FREQ_FINE set?

Hello,

How is the INTERNAL_FREQ_FINE register set in the ISM330?

Is it factory calibrated or is there on board logic that allows it change with age/temp/etc.?

Thank you,

Brandon M

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jan 29, 2025 10:59 AM UTC

Hi @BrandonM ,

I confirm you that also for ISM330 the INTERNAL_FREQ_FINE is factory calibrated.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

BrandonMAuthor
Associate
Jan 27, 2025 9:53 PM UTC

Update : I found a post from Wellett "IIS3DWB - ODR Accuracy" where the same question is asked relating to the IIS3DWB. The response from Federica Bossi says it is set at the factory.

I presume this would be similar for the ISM330.

If this is the case, then since INTERNAL_FREQ_FINE is only set once, that means it does not change with temperature or age of the device.

Presuming 25 Celsius is the measurement point for the standard (based on Federica's response), the accuracy can be +/- 0.5% at 85 C and +/- 0.65% at -40 C.

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jan 29, 2025 10:59 AM UTC

Hi @BrandonM ,

I confirm you that also for ISM330 the INTERNAL_FREQ_FINE is factory calibrated.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
BrandonMAuthor
Associate
Jan 29, 2025 1:01 PM UTC

Thank you