Skip to main content
This topic has been closed for replies.

30 replies

Kabron
Associate II
Feb 1, 2019 4:20 PM UTC

I join to question.

AVARG.2
Visitor II
Feb 4, 2019 4:53 AM UTC

What is the idea behind people counting using VL53L1X sensor Since this sensor is used for measuring the distance. How to detect whether the obstacle is people or not?

Kabron
Associate II
Feb 4, 2019 6:38 AM UTC

I guess they use more than one ROI SPAD regions, but it is beyond current API

Kabron
Associate II
Feb 5, 2019 6:08 AM UTC

I did it! It is very simple.

Unlike ST I will not keep mysterious silence and will publish the code after some tests.

Kabron
Associate II
Feb 5, 2019 12:27 PM UTC

This example illustrates direction recognition with the single VL53L1X TOF sensor. Two Regions Of Interest(ROI) are defined in SPAD sensor array:

 ROI1 ROI2

0,15___12,15 

 ####----####

 ####----####

 ####----####

 ...

 ####----####

 ####----####

_____3,0 _____15,0

Data measurements distance0 and distance1 cyclically readed from both ROIs, switching them on the fly.

Then STM32duino_Proximity_Gesture library used for event interpretation.

To suit Arduino requirement I added necessary library description to Pololu vl53l1_api.

Also, to handle handMustCoverBoth parameter support in STM32duino_Proximity_Gesture library, I had to slightly modify tof_gestures_DIRSWIPE_1.cpp and tof_gestures_DIRSWIPE_1.h. Both libraries are included in this bundle.

This code is for WEMOS D1 mini Lite, but with board and pins adjustments will work with any Arduino.

Data outputs to serial @115200 and to OLED. For investigations and adjustments it is suitable to use SerialPlot: https://bitbucket.org/hyOzd/serialplot.

Files here:

https://yadi.sk/d/UIIAXFol3P_jXg

Video here: 

https://www.youtube.com/watch?v=_ZjAZ7eieNM0690X000006DO9dQAG.jpg0690X000006DO9TQAW.jpg

AVARG.2
Visitor II
Feb 6, 2019 4:04 AM UTC

Thanks for sharing your source code. I am using Nucleo - F401RE board with VL53L1X sensor. Is it possible to use this code in stm nucleo board?

Kabron
Associate II
Feb 6, 2019 6:49 AM UTC

Sure.

You can adapt SimpleRanging example code (from STM32CubeExpansion_53L1A1_V2.0.1) to suit the task.

AVARG.2
Visitor II
Feb 6, 2019 9:59 AM UTC

Actually my doubt is when the sensor detects something , how we identify its a people or not. This sensor detects anything so how we distinguish them?

CNiev
CNievAuthor
Associate
Feb 7, 2019 8:49 AM UTC

Thanks for sharing! This is very interesting!

I understand you made some changes to standard libraries.

Have you considered submitting a patch so it gets integrated in the library?

Kabron
Associate II
Feb 7, 2019 11:35 AM UTC

No, but "Both libraries are included in this bundle."

AVARG.2
Visitor II
Feb 11, 2019 5:04 AM UTC

In that people counting video, they have shown that they have specified some person detection distance range. How this range can be obtained?

Kabron
Associate II
Feb 11, 2019 6:28 AM UTC

How they did it I do not know as their code is not available.

In my variant range defined as:

int tof_gestures_initDIRSWIPE_1(int32_t rangeThreshold_mm, long minSwipeDuration, long maxSwipeDuration, bool handMustCoverBoth, Gesture_DIRSWIPE_1_Data_t *data)

legeardp
ST Employee
Apr 8, 2019 11:08 PM UTC

Hi,

The source code is not available yet on www.st.com but will be made available in the coming weeks.​

If you can't wait please email me : philippe.legeard@st.com

Kabron
Associate II
Apr 9, 2019 7:00 AM UTC

Basing on the current ST answer-speed, we could estimate appearing of the source code in the next few years.