Skip to main content
Pasi MYLLYMAKI
ST Employee
Mar 3, 2021 4:17 PM UTC
Solved

Is the inclinometer calibrated by ST? Why should I buy an expensive inclinometer if I have to calibrate it on my production line?

..

    This topic has been closed for replies.
    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:42 PM UTC

    yes, the inclinometer is accurately calibrated in our factory before being shipped, however, whatever MEMS sensor is influenced by thermal mechanical stresses like the one that happen during the soldering on the PCB of the final product. The necessity of performing a further calibration at the end of the line depends on the accuracy requirements of the applications, but when such requirements are on the high side, you can't practically skip the calibration after soldering and assembly of the final product. What differentiate a low cost accelerometer from an high performance, higher cost inclinometers is mainly the stability and repeatability over temperature and overtime which is something that you can't achieve on low cost accelerometer, even performing more complex and costly calibration over temperature in the factory

    1 reply

    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:42 PM UTC

    yes, the inclinometer is accurately calibrated in our factory before being shipped, however, whatever MEMS sensor is influenced by thermal mechanical stresses like the one that happen during the soldering on the PCB of the final product. The necessity of performing a further calibration at the end of the line depends on the accuracy requirements of the applications, but when such requirements are on the high side, you can't practically skip the calibration after soldering and assembly of the final product. What differentiate a low cost accelerometer from an high performance, higher cost inclinometers is mainly the stability and repeatability over temperature and overtime which is something that you can't achieve on low cost accelerometer, even performing more complex and costly calibration over temperature in the factory