Skip to main content
leandropg
Visitor II
May 11, 2022
Question

Is possible that the LIS2DW12 accelerometer reports via interrupt pin the Single and Double Tap condition at the same time?

Hi,

I am developing an application using the accelerometer LIS2DW12. I need detect the single and double tap at the same time and indicate it to the microcontroller via interrupt pin what condition was detected.

I have could detect single tap and double tap independently and it worked. However when I enable the two conditions (single and double tap) I can't obtain the conditions using a pin interrupt :( . Is like if isn't possible send the two conditions at the same time.

I found it in the manual:

If latch mode is enabled and the interrupt signal is driven to the interrupt pins, the value assigned to SINGLE_DOUBLE_TAP also affects the behavior of the interrupt signal: when it is set to 0, latch mode is applied to the single-tap interrupt signal; when it is set to 1, latch mode is applied to the double-tap interrupt signal only

The manual show examples to Single or Double Tap separate but doesn't at the same time.

Is a limitation of the device? Is not possible detect the two events via interrupt? What another way can I implement to achieve it?

Thanks in advance.

    This topic has been closed for replies.