Skip to main content
NSharp
Associate II
October 25, 2019
Question

Is it possible to use the LSM6DSL accelerometer with a non-Cortex-M3 or -M4 STM32 MCU?

All of the examples of usage that I have seen for the LSM6DSL have been with the STM32 Cortex-M3 and -M4 microcontrollers. I assume that is due to the library calculations that must be made in the support library for this accelerometer/gyro.

Is it possible to use the LSM6DSL as just a simple wake-up interrupt for a Cortex-M0 (STM32L0) controller? I don't need to know, for example, whether a person is standing or walking or running; I just need to know they've moved (within some reasonable tolerance).

This topic has been closed for replies.

2 replies

S.Ma
Principal
October 26, 2019

These are SPI xor I2C devices with little computation on top.

8 bit MCUs like STM8 have even compiler provided math float libraries.

So, technically, it would only be a matter of latency time.

NSharp
NSharpAuthor
Associate II
October 28, 2019

I am not even looking at doing any calculation with the data. Rather, I am simply looking for a way to wake the MCU based on the wake-up interrupt from the LSM6DSL.