Skip to main content
SM.19
Visitor II
August 20, 2019
Question

Is it Possible to use Accelerometer(IIS2DLPC) for Angle Measurement in Vibrating Medium ??

I am using IIS2DLPC accelerometer for Angle Measurement .

My Question is :

Whether it is Advisible to use II2DLPC for Angle Measurement, when the IIS2DLPC is Placed on the Vibrating Object ??.

Example Scenario :

If a shaft( IIS2DLPC is placed on the Shaft) is Fitted inside the Car, Is it possible to Measure the Tilt Angle of the Shaft when the Car is in the Movement ??

    This topic has been closed for replies.

    3 replies

    Eleon BORLINI
    ST Employee
    September 4, 2019

    ​Hi @SM.19​ , if the vibration object produces a noise which hasn't significant DC component, you can set a low ODR and a LPF filter (e.g. LPF2, p.30 del datasheet) which works at ODR/4 and enables you to reject the in-band noise. Btw, I suggest you to try to work in an as much as possible controlled environment, because accuracy can vary with temperature. Regards

    MKear
    Associate
    September 6, 2019

    I say No. Accelerometers become quite impossible on anything which is fast moving or vibrating. You need an gyro as well, combining the two with sensor fusion. The outcome is 1000 times better. We've recently spent lots of time arriving at this conclusion. The Matlab imufilter() function is a good place to start.

    Eleon BORLINI
    ST Employee
    September 17, 2019

    The better ST sensor for tilt measurement is IIS3DHHC, a precision inclinometer which focuses on this kind of application. Btw, if you have the possibility to implement a sensor fusion / IMU with a 6axis module, this will sure be of your help. Regards​