Skip to main content
ACand.3
Associate III
Jun 9, 2025 5:43 PM UTC
Solved

Is it possible to run FIFO data and MLC at the same time for the lsm6dsv16x?

I followed most of the examples to get data such as accel, gyro, timestamp and temperature from the github repo using fifo interrupts. I also used the mlc_gym example to get data from a MLC configuration that I designed on Mems studio. 

 

My question is, can I use both configurations at the same time? like have an interrupt for the fifo data ready and one interrupt for the MLC? 

As in, I am constantly reading raw accel/gyro/timestamp/temp data at a fixed 60Hz on interrupt 1 and also get a new MLC state on interrupt 2?

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jun 12, 2025 9:38 AM UTC

Hi @ACand.3 ,

Yes, you can use an interrupt for the FIFO and the other one for the MLC at the same time.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jun 12, 2025 9:38 AM UTC

Hi @ACand.3 ,

Yes, you can use an interrupt for the FIFO and the other one for the MLC at the same time.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.