Skip to main content
NShar.19
Associate
September 27, 2021
Question

Is it possible to communicate LSM6DSL and MCU via SPI, when CS pin in LSM6DSL is hardware fix as GND, and MCU do not control it. As I read in datasheet this pin is for choosing a interface, SPI or I2C.

  • September 27, 2021
  • 1 reply
  • 780 views

..

This topic has been closed for replies.

1 reply

TBomb.1
Visitor II
October 7, 2021

Hi, yes, if you are only interested in the SPI communication, the CS pin can be forced low all the time. Check however if this increases the current consumption in power down in case the CS pin would be internally pulled up (but no mention of this on the datasheet).

\Tom