The FSM/MLC configuration generated with our tool is specific for ST sensors. However, a similar model could be created to run on MCU as well.
For the integration of the FSM / MLC configuration in a specific driver / firmware, you can reference to the Platform independent drivers in our GitHub repository --> LINK
If you navigate in the LSM6DSOX folder, you can find some examples of integration of .h files containing FSM / MLC configurations.
It is also possible to combine the model which is running in the sensor with a model running in the MCU. For instance, a simple model running on the sensor (at very low current consumption) generates an interrupt on specific conditions to trigger the MCU. The MCU can run a more complex model when triggered by the sensor, staying in sleep mode most of the time in order to further reduce the overall current consumption of the sensor+MCU solution.