Skip to main content
luisf
Associate II
February 23, 2017
Question

Is CTRL_REG0 on LIS3DH available since the beginning?

Posted on February 23, 2017 at 02:39

Hi, I have a project that uses LIS3DH. I just noticed an update at the Datasheet and now there is a  CTRL_REG0 that I can disable the SA0 pull-up. Is this available since the beginning or just on new batches of the device?

    This topic has been closed for replies.

    2 replies

    ST Employee
    February 23, 2017
    Posted on February 23, 2017 at 09:14

    It is available since the beginning.

    luisf
    luisfAuthor
    Associate II
    April 25, 2017
    Posted on April 25, 2017 at 21:51

    Thank you. Is there any special procedure or timig restriction to disable the pull-up? I am using the LIS3DH with the SPI and i see some current leakage with the pull-up? Sometimes i send the command and the current goes away and sometimes it dont.