Skip to main content
thorben k
Visitor II
October 10, 2017
Question

Interrupts arent working

Posted on October 10, 2017 at 15:14

 i am working with the LSM9DS1.

I want to read the accelerometer data using interrupts. The problem is that, when i enable the 'data ready interrupt'(INT_DRDY_XL) and read and printf STATUS_REG, to see whether one or more interrupts have been generated, it gives me back 0b00000101 . But it should be 0b10000101 because a new interrupt should have been generated.

my sensor register are:

void init_accel_interrupt(void){

    uint8_t reg_value =0;

    reg_value = 0x07 << 3;  // x,y,z axis enabled

    write_reg(CTRL_REG5_XL,reg_value);

    reg_value = 0;

    reg_value = (0x06 << 5); // 952 Hz odr

    reg_value|= (0x02 << 3); // +-4g

    reg_value|= (0x01 << 2); // bw select according to bw[1:0]

    reg_value|= (0x00 << 0); //408 hz bw

    write_reg(CTRL_REG6_XL,reg_value);

    reg_value = 0;

    reg_value = (0x01 << 7);// high resolution

    reg_value|= (0x03 << 5); // cutofffrequency odr/50= 0 odr/100 =1 odr/400=3

    reg_value|= (0x01 << 2); // filter enabled

    write_reg(CTRL_REG7_XL,reg_value);

    reg_value = (0x01 << 0);

    write_reg(INT1_CTRL,reg_value);    // data ready interrupt int1

    reg_value = (0x01 << 0);

    write_reg(INT2_CTRL,reg_value);  // data ready interrupt int2

    reg_value = (0x01 << 4) | (0x01 << 5) ;// open drain, active low

    write_reg(CTRL_REG8,reg_value);

    reg_value = (0x01 << 3);        // data available timer enabled

    write_reg(CTRL_REG9,reg_value);

}

and my loop is:

     while (1){

 

             rv = read_reg(STATUS_REG_0);//

             printf_P(PSTR('%i  \n'),rv);

             rv = read_reg(STATUS_REG_1);//

              printf_P(PSTR('%i  \n'),rv);

             rv = read_reg(INT_GEN_SRC_XL);//

             printf_P(PSTR('%i  \n'),rv);

            _delay_ms(1);

output is : 5

                 5

                 0

This topic has been closed for replies.

1 reply

ST Employee
October 10, 2017
Posted on October 10, 2017 at 16:28

The bit IG_XL in the STATUS_REG will not be set by 

data ready. Accelerometer data ready signal controls the XLDA bit.

The IG_XL bit would be set by interrupt from interrupt generator configured in INT_GEN_CFG_XL register which you don't use.

0690X00000608YAQAY.png