Question
Interrupt GPIO VL53L0X
Posted on February 21, 2018 at 14:47
hi,
how does the Vl53L0X ranging sensor adress the GPIO for the interrupt, i can only find a long list of register adresses in the vl53l0x_interrupt_threshold_settings.h.
After initialization and calibration of the Sensor, i tried it with the code below. However, no interrupt is given out in StartMeasurement(). Im using the stm32f103RE microcontroller.
FixPoint1616_t threshold_high=(255);
FixPoint1616_t threshold_low=(350);status= VL53L0X_SetInterruptThresholds(pTestDev,
VL53L0X_DEVICEMODE_SINGLE_RANGING, threshold_low , threshold_high); status=VL53L0X_SetGpioConfig(pTestDev,0,VL53L0X_DEVICEMODE_SINGLE_RANGING,VL53L0X_GPIOFU NCTIONALITY_THRESHOLD_CROSSED_LOW, VL53L0X_INTERRUPTPOLARITY_LOW);status=VL53L0X_StartMeasurement(pTestDev);
best regards
jonas
#interrupt #vl53l0x #stm32f103 #interrupt-status-register