Skip to main content
AB.4
Associate III
February 5, 2019
Question

Interrupt generation for activity event

Hello,

I have configured LIS2DH12 to generate interrupt on INT2 pin on activity as well as a strong impact using the register values as follows:

CTRL_REG1 - 0x37

CTRL_REG2 - 0x00

CTRL_REG3 - 0x40

CTRL_REG4 - 0x88

CTRL_REG5 - 0x0A

CTRL_REG6 - 0x28

INT1_THS - 0x16

INT1_DUR - 0x0C

INT1_CFG - 0x95

INT2_THS - 0x70

INT2_DUR - 0x01

INT2_CFG - 0x2A

ACT_THS - 0x10

ACT_DUR - 0x20

With this configuration, I would like to know regarding the interrupt generation for activity. 1. Does the interrupt get generated for both sleep to wake transition event as well as wake to sleep transition event?

2. Also, when the sleep to wake transition occurs, does the INT2_SRC register set the one or more of the bits ZH, YH & XH?

3. And when the wake to sleep transition occurs, does the INT2_SRC register set one or more of the bits ZL, YL & XL?

4. Does duration set in ACT_DUR apply for both sleep to wake event and wake to sleep event?

Can you please provide your inputs on this?

Thanks in advance.

Regards,

Anusha

This topic has been closed for replies.