Skip to main content
SAgaz.1
Associate II
August 12, 2021
Question

Interfacing with onboard i3g4250d gyroscope on STM32F429i

  • August 12, 2021
  • 2 replies
  • 2820 views

I have been trying to test and get the gyroscope to communicate via SPI for a bit however it just seems to *refuse* to respond. As per the User manual for the board UM1670, PC1 is CS, PF7 is the serial clock, PF8 is MISO, and PF9 is MOSI all for SPI5. I suspect something is wrong with my setup of pins but I cant find what, so far I have:

Enabled the SPI5 clock as well as Port C and Port F clocks.

Configured PF7-9 as AF5, no pull.

Configured PC1 as general purpose output with no pull, and then set it to high in ODR (Since CS is high by default). Then I initiate SPI5 and begin by trying to send 2 bytes of data, 0x20 and then 0xf to the Gyro's CTRL1 register. After that as a test I keep trying to get info from the WHO AM I register just to test communication.

The only thing I get on the SPI bus is the value '255', which I assume is just all 1s. I used a logic analyzer to see what was happening and saw no activity on the MISO line.

I can't seem to understand if theres something I am missing with initializing communication with the gyroscope, or am I missing something with initializing the SPI. Here are the relevant code sections:

Relevant initialization code:

__HAL_RCC_GPIOC_CLK_ENABLE();
	__HAL_RCC_GPIOF_CLK_ENABLE();
	__HAL_RCC_SPI5_CLK_ENABLE();
	GPIO_InitTypeDef GPIO_InitStruct; //SPI Pins
	GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI5;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
	
	GPIO_InitTypeDef GPIO_InitStruct1; //Chip Select Pin
	GPIO_InitStruct1.Pin = GPIO_PIN_1;
	GPIO_InitStruct1.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct1.Pull = GPIO_NOPULL;
	GPIO_InitStruct1.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(GPIOC, &GPIO_InitStruct1);
	GPIOC->ODR |= (1 << 1);
	
	mySPI5.Instance = SPI5;
	mySPI5.Init.Mode = SPI_MODE_MASTER;
	mySPI5.Init.Direction = SPI_DIRECTION_2LINES;
	mySPI5.Init.DataSize = SPI_DATASIZE_8BIT;
	mySPI5.Init.CLKPolarity = 2;
	mySPI5.Init.CLKPhase = SPI_PHASE_1EDGE;
	mySPI5.Init.NSS = SPI_NSS_SOFT;
	mySPI5.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
	mySPI5.Init.FirstBit = SPI_FIRSTBIT_MSB;
	mySPI5.Init.TIMode = SPI_TIMODE_DISABLE;
	mySPI5.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
	mySPI5.Init.CRCPolynomial = 10;
	if (HAL_SPI_Init(&mySPI5) != HAL_OK)
	{
		asm("bkpt 255");
	}
	

Call order in main

HAL_Init();
	SysTick_Config(SystemCoreClock / 1000);
	SystemClock_Config();
	
	SPI5_Init();
	UART1_Init();
	GYRO_Init();
static void GYRO_Init(void) {
	GPIOC->ODR &= ~(1 << 1);	
	HAL_SPI_Transmit(&mySPI5, test, 2, 10);
	while (mySPI5.State == HAL_SPI_STATE_BUSY_TX) ;
	GPIOC->ODR |= (1 << 1);
	
	
}

infinite while loop regarding pinging the who am I register (address 0x0f)

while (1) {		
		GPIOC->ODR &= ~(1 << 1);	
		HAL_SPI_TransmitReceive(&mySPI5, 0x0f, buffer_rx , 1, 1);
		while (mySPI5.State == HAL_SPI_STATE_BUSY_TX);
		GPIOC->ODR |= (1 << 1);	
	}

This topic has been closed for replies.

2 replies

SAgaz.1
SAgaz.1Author
Associate II
August 12, 2021

0693W00000D2EZtQAN.pngsomething else I just noticed while looking at the logic analyzer, is other than the fact that MISO (D4) does not even move (likely the reason why I only get 0xFF returned back to the master) the clock movement (D2) seems a bit not only erratic when it goes down, but duty cycle seems very very slow, though I am using the default STCUBEMX SPI initiation settings.

TBomb.1
Visitor II
August 12, 2021

Hi, instead of starting a code from scratch (with CubeMX), you can refer to the MEMS_Example you can find in the STSW-STM32138: STM32F429 discovery firmware package (UM1662).

https://www.st.com/en/embedded-software/stsw-stm32138.html

You can start from this and modify the code for the i3g4250d.

https://www.st.com/resource/en/datasheet/i3g4250d.pdf

Tom