Skip to main content
Associate II
Aug 6, 2025 7:20 AM UTC
Question

Interfacing MP34DT06 with STM32F401RE Sensor

Hi,

I’m using the NUCLEO-STM32F401RE with the X-NUCLEO-CCA02M2 board, which has two MP34DT06 PDM microphones. 

I want to capture stereo audio using I2S2 and convert it to PCM using the PDM2PCM middleware in STM32CubeIDE.

In AN5027 (page 18), a timer is used for stereo mode. This confuses me — since I2S2 can generate the clock and receive data, is the timer still needed to capture stereo PDM signals?

I’m new to this domain, so any guidance is appreciated.

Thanks!

This topic has been closed for replies.