Skip to main content
thomaspietrzak9
Associate II
October 9, 2013
Question

iNemo M1 firmware?

Posted on October 09, 2013 at 10:07

Hi guys,

I just received a couple of iNemo M1 boards (http://www.st.com/web/en/catalog/sense_power/FM89/SC1448/PF253162). It's a nice little gem, and I look forward to design great stuff with it. However I have not managed to talk to it yet. So far I managed to upload iNEMOV2_Firmware_PackageV2.2.0_AHRS through USART, but I got no data when listening, and it was not recognized by the demo application.

Looks like there are: iNEMOEngine_PW8, iNEMOEngine_Ll3, iNEMOEngine_PAAP and iNEMOEngine_Pl3P, but I could not find the files� Moreover my goal is to change the firmware, so I believe I need the Light version provided with sources.

So in brief, is there a working firmware and demos somewhere? Is there firmware example sources somewhere? Should I use a different communication port?

Thank you very much

#inemo-m1-firmware-demos-source
    This topic has been closed for replies.

    1 reply

    zjh
    Visitor II
    January 8, 2015
    Posted on January 08, 2015 at 17:36

    Hi,I got the inemo-m1li3 from the MyST. When you save it to your space, and then you build a project. After that, they will confirm you if you can download maybe after 1 hour.