Skip to main content
mikem
Visitor II
March 27, 2016
Question

Incorrect FIFO alignment

Posted on March 27, 2016 at 01:02

I am running the LSM6DS3 in continuous FIFO mode capturing gyro and acc data. While collecting data I periodically pole to see if the water mark is met (96 words), and if so read out half of them (leaving some in the FIFO). Every once in a while (seeming randomly) the data seems to be misaligned, meaning all the data for one ''sample'' of 6 words is shifted. I get acc_Z in acc_Y and acc_Y in gyro_Z. The next read the data seems to be back to where it should be. How do I ensure the FIFO alignment during FIFO reads?

I am running at 800Hz, no decimation, Acc and Gyro data, reading via SPI at full speed. 

#lsm6ds3-fifo-alignment
This topic has been closed for replies.