Skip to main content
Mk.7
Visitor II
August 18, 2022
Question

in LSM6DS3TR The accelerometer is activated from power-down by ODR_XL[3:0] in CTRL1_XL (10h) the gyroscope is activated from power-down by ODR_G[3:0] in CTRL2_G (11h). For combo-mode what we have to do?

  • August 18, 2022
  • 1 reply
  • 943 views

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    August 25, 2022

    Hi @Mk.7​ ,

    to activate both devices (combo mode), you can just set ODR_XL[3:0] and then ODR_G[3:0] in sequence. You can refer for example to Github sample code --> lsm6ds3_read_data_polling.c

     /* Set full scale */
     lsm6ds3_xl_full_scale_set(&dev_ctx, LSM6DS3_2g);
     lsm6ds3_gy_full_scale_set(&dev_ctx, LSM6DS3_2000dps);
     /* Set Output Data Rate for Acc and Gyro */
     lsm6ds3_xl_data_rate_set(&dev_ctx, LSM6DS3_XL_ODR_12Hz5);
     lsm6ds3_gy_data_rate_set(&dev_ctx, LSM6DS3_GY_ODR_12Hz5);

    -Eleon