Skip to main content
AZakr.1
Associate II
April 30, 2022
Question

In all examples from Hands-on Workshop "Developing with Sensors Made Simple"(pdf) the blue button interrupt is forgotten? Especially in LAB 5?

When I press the blue button, the example applications die :( (especially in LAB 5 where blue is a single or double click switch)

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    ST Technical Moderator
    May 3, 2022

    The Blue Button does trigger an interrupt, but the interrupt function was not used/implemented in Lab5, so pressing it does not lead to any meaningful result.

    However, you have misunderstood the goal of Lab5: Tap and Double Tap are not triggered by the Blue Button, but by the sensor LSM6DSO, which is located on the X-NUCLEO-IKS01A3 used in the Lab.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    AZakr.1
    AZakr.1Author
    Associate II
    May 3, 2022

    Thank you very much for your response.

    Unfortunately, it is probably wrong. Sorry.

    Please read carefully the readme.txt file contained in the LSM6DSO_SingleDoubleTap folder of the X-CUBE-MEMS1 package.

    I will quote you an important passage:

    "After application is started: - the user can try to tap the STM32 Nucleo board; when the single tap is detected, the LED is switched on for a while. Press the user button to pass from the single tap detection to the double tap detection feature. When the double tap is detected, the LED is switched on twice for a while. Press again the user button to disable the single / double tap detection feature. Press the user button to enable again the single tap detection feature and so on. "

    The mode switching functionality described above probably does not work due to a misconfiguration EXTI_line [15:10] interrupt. The same mistake probably occurs in all Hands-on Workshop "Developing with Sensors Made Simple" (pdf) exercises. I am writing probably because I am a novice programmer and I am looking for a competent explanation of this strange situation. I might be wrong. But your explanation is probably superficial.

    If you can, code Lab5 and share the result.

    Regards

    Adam