Skip to main content
SPinj
Associate II
April 9, 2019
Question

Importing libraries from IAR embedde workbanch to Atollic True studio IDE

I want to interface "MP34DT01" mic with "STM32L476VG discovery board" to get ambiant noise level in dBs.

In STM32l476VG firmware packages there is demostaration code which gives sound level or Noise level in dBs.

But In the demonstration code one static library (lib_smr_CM4F) has been used that is only supported by IAR Embedded Workbanch.

I want to import my code in Atollic True studio IDE but I can't due to those static library.

suggest me any firmware or library which can give me microphone output data in dBs in Atollic True studio IDE.

Any little help appreciated.

Thanks Regards,

Sadik pinjari

    This topic has been closed for replies.

    4 replies

    AvaTar
    Senior III
    April 9, 2019

    TrueStudio uses a GCC-based toolchain, so a GCC version of said lib (usually named *.a) should work.

    And yes, due to format differences, gcc, Keil and IAR link-libraries are not directly interchangeable.

    Another option would be to build the lib yourself from the source code - if available.

    SPinj
    SPinjAuthor
    Associate II
    April 10, 2019

    Thanks for your reply.

    GCC version of  static library (lib_smr_CM4F) is not available. can you give me some resources which can help me .

    or suggest me if another firmware or library available which can give PDM signal into dBs.

    AvaTar
    Senior III
    April 10, 2019

    > can you give me some resources which can help me .

    Sorry, no. I would ask ST (distributor or FAE perhaps).

    SPinj
    SPinjAuthor
    Associate II
    April 10, 2019

    ok .

    Thank you.