Skip to main content
Bbile.1
Visitor II
April 6, 2021
Question

im new with stm iar embedded workbench , im working with STM32CubeExpansion_LRWAN_V1.3.1, so i have a prob cant find where is my sensor are declared if anyone can help

..

This topic has been closed for replies.

2 replies

Eleon BORLINI
ST Employee
April 7, 2021

Hi @Bbile.1​ ,

I'm not an expert of this tool, so I added the LoRa topic for more help.c

Checking the I-CUBE-LRWAN firmware function pack (2.0.0 version), I can see that the drivers for the sensors can be found in the \Drivers\BSP\Components.

Then, in the UM2073 user manual at p. 38 there is the End_node application description that might be of your interest: the specific project can be found in the \Projects\B-L072Z-LRWAN1\Applications\LoRaWAN\LoRaWAN_End_Node\EWARM, and the file dedicated to the sensors' configuration should be the sys_sensor.c.

Please note also that you need the X-NUCLEO-IKS01A2 or the X-NUCLEO-IKS01A3 board for sensors' connection.

-Eleon

Tesla DeLorean
Guru
April 7, 2021

Yeah, I don't think the problem here is reach.

The question isn't well stated, and has a random screen shot.

Is it a question of how to drive IAR? Or do static source analysis?

Do you have a supervisor or more senior staff member who can work with you?

Which project specifically within the LRWAN V1.3.1?

On what board or combinations of boards?

Doesn't grep or find-in-files provide some association?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..