Skip to main content
DBass.2
Visitor II
March 27, 2023
Solved

ILPS22QS Cleaning After Soldering

TN0018 calls out in the Process considerations section that the board must be properly cleaned after soldering if "self-cleaning" solder paste is not used. Are there any guidelines on cleaning methods that will not damage the sensor? Can the sensor port be covered with something like Kapton tape to protect it during the cleaning process?

    This topic has been closed for replies.
    Federica Bossi
    Federica BossiBest answer
    ST Technical Moderator
    April 7, 2023

    Hi @DB.7assett​ ,

    Welcome to ST Community!

    There are too many cleaning procedure that are dependent to manufacturer (and sometimes also to the used oven). For pressure sensor devices there are two methodology to use to avoid to damage the device:

    1. don't use the Kapton over the window of device because the glue can close the small holes. 

    2. It is mandatory don't use vapor phase machine for soldering.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster!

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Federica Bossi
    Federica BossiBest answer
    ST Technical Moderator
    April 7, 2023

    Hi @DB.7assett​ ,

    Welcome to ST Community!

    There are too many cleaning procedure that are dependent to manufacturer (and sometimes also to the used oven). For pressure sensor devices there are two methodology to use to avoid to damage the device:

    1. don't use the Kapton over the window of device because the glue can close the small holes. 

    2. It is mandatory don't use vapor phase machine for soldering.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster!

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.