Skip to main content
MRaff.1
Associate III
January 30, 2024
Solved

IKS4A1 eCompass application with Unicleo-GUI

Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI. 

The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 software package for STM32MX".

For some unexplainable (to me) reason, it looks like the board looks for sensors placed on another expansion board I don't have so that I am unable to get sensor data from the magnetometer placed on the IKS4A1.

 

The IKS4A1 magnetometer is placed on the right side of the board. I have not the green board shown in the picture and it seems to me I have not configured it. 

MRaff1_0-1706620923031.png

 

When I open Unicleo the user message tab shows:

 

Port: COM8 Successfully Opened
PresString Received: MEMS shield demo,12,10.0.0,1.5.0,IKS4A1
Firmware Type: E-Compass
Expansion Board IKS4A1 Successfully Initialized

 

but nothing works.

Here my Cube project. 

Any help will be very appreciated. 

Thank you.

 

This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
January 31, 2024

Hello @MRaff.1,

I have analyzed your .ioc file and you have to enable interrupt for TIM3.

MiroslavBATEK_1-1706693931251.png

I recommend you to increase stack size as well.

MiroslavBATEK_2-1706693970154.png

After that it works as expected.

There is a bug in Unicleo-GUI which displays a DIL24 adapter even if it is not used, but this is only graphical issue, all the remaining functions work well. Anyway I would recommend you to use MEMS Studio which is our new tool.

MiroslavBATEK_3-1706694224930.png

 

 

 

 

 

2 replies

Miroslav BATEKBest answer
ST Employee
January 31, 2024

Hello @MRaff.1,

I have analyzed your .ioc file and you have to enable interrupt for TIM3.

MiroslavBATEK_1-1706693931251.png

I recommend you to increase stack size as well.

MiroslavBATEK_2-1706693970154.png

After that it works as expected.

There is a bug in Unicleo-GUI which displays a DIL24 adapter even if it is not used, but this is only graphical issue, all the remaining functions work well. Anyway I would recommend you to use MEMS Studio which is our new tool.

MiroslavBATEK_3-1706694224930.png

 

 

 

 

 

MRaff.1
MRaff.1Author
Associate III
January 31, 2024

Thank you Miroslav, set the TIM3 interrupt and increased the stack size, installed MEMS-Studio and now everything is fine. I am very happy. Thank you!!!!