Skip to main content
HKim.23
Associate III
March 12, 2024
Question

[iis3dwb] What are the units of the BDR_XL registor?

Adjusting the register values below seems to adjust the time at which data is written to the buffer.

HKim23_0-1710207022327.png

 

I understood that the value is similar to Data Sampling frequency.

If i set the value to 6, about 1900 data per second will be written to the buffer.
I would like to know the exact units of that value.

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
March 12, 2024

Hi @HKim.23 ,

It is the batching data rate and the unit is Hz.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
HKim.23
HKim.23Author
Associate III
March 12, 2024

if BDR_XL is 0b1010, Batching Data Rate is 26667Hz.

Then, if BDR_XL is 0b0110, what is the Batching Data Rate?

 

Federica Bossi
ST Technical Moderator
March 26, 2024

Hi @HKim.23 ,

As written in the application note, the only two possible configurations are 0000 (default) or 1010 (26667Hz):

 

FedericaBossi_0-1711457416978.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.