Skip to main content
Visitor II
Oct 1, 2025 6:14 PM UTC
Solved

iis3dwb issue while capturing data max data-rate

Hi,

I am trying to capture data from the IIS3DWB sensor at its maximum rate and save it into a buffer of length 8192 (due to internal RAM limitations). I'm using SPI with DMA to interface with the sensor. However, I'm not able to capture the data correctly — the X-axis shows incorrect values, while the Y and Z axes remain constant. I tested with another sensor, but the issue persists. The FIFO is configured to stream mode. I haven't detected any buffer overflows. I'm attaching the code and a CSV file for reference.

 SETTINGS: SPI clock-8MHz, iis3dwb stores data in FIFO in continuous mode with 26.67k ODR , 3-axis mode is used, timestamp batch to FIFO is on, BDU is on, 16G range mode is on, IRQ pin -not connected, using polling mode. 

can anyone give me solution.

 

Thanks 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 7, 2025 9:43 AM UTC

Hi @ajaya_kumar ,

You have enabled timestamp batch with iis3dwb_fifo_xl_batch_set(&dev_ctx, IIS3DWB_XL_BATCHED_AT_26k7Hz);

This means every N samples, 3 bytes of timestamp data are inserted into the FIFO stream. Your current parsing assumes all FIFO entries are 6-byte accelerometer samples, but with timestamp batch enabled, some entries are 9 bytes (6 accel + 3 timestamp).

This mismatch causes misalignment in reading axis data.

The SAMPLE_COUNT should reflect the number of FIFO entries, not just accelerometer samples, because timestamp batches occupy FIFO space.

The actual number of accelerometer samples will be fewer than SAMPLE_COUNT if timestamp batching is enabled.

To simplify debugging, temporarily disable timestamp batching: this will make all FIFO entries pure accelerometer samples (6 bytes each), so your current parsing logic will work correctly.

 
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 7, 2025 9:43 AM UTC

Hi @ajaya_kumar ,

You have enabled timestamp batch with iis3dwb_fifo_xl_batch_set(&dev_ctx, IIS3DWB_XL_BATCHED_AT_26k7Hz);

This means every N samples, 3 bytes of timestamp data are inserted into the FIFO stream. Your current parsing assumes all FIFO entries are 6-byte accelerometer samples, but with timestamp batch enabled, some entries are 9 bytes (6 accel + 3 timestamp).

This mismatch causes misalignment in reading axis data.

The SAMPLE_COUNT should reflect the number of FIFO entries, not just accelerometer samples, because timestamp batches occupy FIFO space.

The actual number of accelerometer samples will be fewer than SAMPLE_COUNT if timestamp batching is enabled.

To simplify debugging, temporarily disable timestamp batching: this will make all FIFO entries pure accelerometer samples (6 bytes each), so your current parsing logic will work correctly.

 
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.