Skip to main content
Mark Hughes
Visitor II
June 8, 2018
Question

IIS3DHHC When used as an inclinometer, what is the minimum angular resolution?

  • June 8, 2018
  • 0 replies
  • 560 views
Posted on June 08, 2018 at 23:30

The IIS3DHHC is a triaxial accelerometer that outputs 16-bit data, 3-axis, �2.5 g acceleration data.

So (5g)/(2^16 bits) = 7.63*10^-5 g's/LSB.

arctan(7.63*10^-5) is essentially the same thing (small angle approximation in radians)

and that converts out to 0.00437 degrees -- which is about 0.2622 arc-minutes -- which is about 15.74 arc-seconds.

So the LSB represents about 16 arc-seconds of resolution -- is that correct?

The other way I can talk myself into a solution is to eliminate 1 bit for the sign -- leaving 15 bits for a full scale value.  As an inclinometer, I'd never expect the value to exceed 1g -- so now we're down to 14 bits corresponding to 1g.

arctan(1/10^14)=12.5 arcseconds.

At the same time, I see that there is a 2%FS non-linearity -- thats 10-11 bits of data.  Where is the deviation the greatest, and how does that affect the usefulness of this device as an inclinometer?  By my count -- I'm down to 3-4 bits of reliability.

Thanks,

Mark

#accelerometer #iis3dhhc #mems
This topic has been closed for replies.