Skip to main content
HTaka.8
Visitor II
September 30, 2019
Question

IIS2MDCTR temperature rating.

Please present the junction temperature rating of IIS2MDCTR,

Is it generally the same as the storage temperature?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    October 4, 2019

    Hi @HTaka.8​ , please check if I well interpreted you question. The IIS2MDCTR max supply is 3.6V and max current (high performance mode, max ODR) is 1130uA, so the power consumed in the worst case is P=V*I=4mW. If you consider that the device package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. Moreover, no worry about the junction temperature with respect to storage temperature. Regards