Skip to main content
Visitor II
Sep 8, 2025 9:27 AM UTC
Question

IIS2MDC makes false detection after some time on the road

I am developing a wireless sensor to detect vehicles using the IIS2MDC. My main logic is:

BOOT -> Init sensor -> Measure environment -> Set detection thresholds and offsets based on environment -> Set interrupts -> Wait for interrupt

 

On interrupt -> Acquire vehicle heading -> Send RF signal to gateway


After some hours working properly the sensor starts sending continuous signals without a vehicle or other metalic object nearby. How can i correct this behaviour? Any help is welcomed.

 

Below i'll leave the application code for the IIS2MDC initialization:

 

CFG_REG_A is always 0x90

CFG_REG_B is always 0x09

CFG_REG_C is always 0x50

INT_CTRL_REG is 0x00 on startup and 0x45 on work mode

 

#define IIS2MDC_STARTUP_CFG 		{0x90, 0x09, 0x50, 0x00}
#define IIS2MDC_WORK_CFG 		{0x90, 0x09, 0x50, 0x45}

bool iis2mdc_startup_mode() {
 uint8_t dev_id = 0;
 bool error = iis2mdc_i2c_read(WHO_AM_I, &dev_id, 1);

 if (dev_id != DEVICE_ID || error) return false;

 uint8_t cfg_reg_a = (1<<5); // soft reset
 if (iis2mdc_i2c_write(CFG_REG_A, &cfg_reg_a, 1)) return false;

 Task_sleep(5);

 cfg_reg_a = (1<<6); // reboot
 if (iis2mdc_i2c_write(CFG_REG_A, &cfg_reg_a, 1)) return false;

 Task_sleep(MS_TO_TICKS(20));

 uint8_t config[4] = IIS2MDC_STARTUP_CFG;
 if (iis2mdc_i2c_write(CFG_REG_A, config, 4)) return false;

 return true;
}

bool iis2mdc_work_mode() {
	uint8_t config[4] = IIS2MDC_WORK_CFG;
	if (iis2mdc_i2c_write(CFG_REG_A, config, 4)) return false;

	return true;
}

bool iis2mdc_learn() {
	uint8_t i = 0;
	int64_t x = 0;
	int64_t y = 0;
	int64_t z = 0;

	while (i < REF_SAMPLES) {
		uint8_t status = 0;
		if (iis2mdc_i2c_read(STATUS_REG, &status, 1)) return false;

		if (status & 0x08) {
			MagneticRawData_t raw_data = {0,0,0};
			if (iis2mdc_i2c_read(OUTPUT_REG, (uint8_t*)&raw_data, OUTPUT_REG_LEN)) return false;

			x += raw_data.x;
			y += raw_data.y;
			z += raw_data.z;

			i++;
		}
	}

	x = x / REF_SAMPLES;
	y = y / REF_SAMPLES;
	z = z / REF_SAMPLES;

	int16_t offsets[3] = {x,y,z};
	iis2mdc_i2c_write(OFFSET_REGISTER, (uint8_t*)offsets, OFFSET_REG_LEN);

	uint16_t mag = 4 * sqrt(y*y + z*z) / REF_SAMPLES;
	if (iis2mdc_i2c_write(INT_THRESH_REG, (uint8_t*)&mag, 2)) return false;


	return true;
}

void main() {
 // Abstracted main
 iis2mdc_startup_mode();
 iis2mdc_learn();
 iis2mdc_work_mode();
 
 // Start a task that is released on interrupt
 // and send the RF signal
}

 

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
Sep 11, 2025 12:46 PM UTC

Hi @francsicosousa ,

Can you log the magnetic sensor output during the operation to check if the output data is drifting, causing the threshold to be not valid anymore? 

If this is the case, you can achieve a more stable sensor output by enabling the automatic offset compensation feature. It can be enabled by setting bit 2 of reg CFG_REG_B to '1'.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.