Skip to main content
Associate III
Oct 28, 2025 3:42 AM UTC
Question

iis2iclx fifo only trigger once

I want to read the FIFO of IIS2ICLX, but I found that INT1 only triggers once when the power is first turned on. This is my initialization code. Is there anything wrong with this initialization?

I triggered the interrupt through the rising edge. Once the interrupt occurred, an event would be sent. I measured the level of the interrupt pin, and it remained constant.

iis2iclx_xl_full_scale_set(&dev_ctx, IIS2ICLX_500mg);
/* Configure filtering chain(No aux interface)
* Accelerometer - LPF1 + LPF2 path
*/
iis2iclx_xl_hp_path_on_out_set(&dev_ctx, IIS2ICLX_LP_ODR_DIV_10);
iis2iclx_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);

iis2iclx_fifo_xl_batch_set(&dev_ctx, IIS2ICLX_XL_BATCHED_AT_104Hz);
iis2iclx_xl_data_rate_set(&dev_ctx, IIS2ICLX_XL_ODR_104Hz);
s_sample_rate = 104.0f;
iis2iclx_fifo_watermark_set(&dev_ctx, 112);
iis2iclx_fifo_mode_set(&dev_ctx, IIS2ICLX_FIFO_MODE);
iis2iclx_pin_int1_route_t int1_route;
int1_route.int1_ctrl.int1_fifo_th = 1;
int1_route.int1_ctrl.int1_fifo_ovr = 1;
int1_route.int1_ctrl.int1_fifo_full = 1;
int1_route.int1_ctrl.int1_cnt_bdr = 1;
iis2iclx_pin_int1_route_set(&dev_ctx, &int1_route);​

 

This topic has been closed for replies.

3 replies

Alpha_LeeAuthor
Associate III
Oct 28, 2025 8:04 AM UTC

i tryed INT2, it have same probelm

Federica Bossi
ST Technical Moderator
Oct 28, 2025 2:50 PM UTC

Hi @Alpha_Lee ,

Try this: start by enabling only int1_fifo_th (watermark interrupt). Test behavior, then add other interrupts as needed.

After INT1 triggers, read the FIFO data or the interrupt status registers to clear the interrupt condition. This will de-assert the INT1 pin and allow new interrupts.

You could also lower the FIFO watermark to a smaller value (e.g., 16 or 32) for more frequent interrupts.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Alpha_LeeAuthor
Associate III
Oct 29, 2025 1:35 AM UTC

I set FIFO watermark 16, and enable only int1_fifo_th, but it still can't work. 

switch (iis2iclx_event)
{
 case EV_FIFO_FULL:
 {
 /* Read output only if new value is available */
 iis2iclx_fifo_status2_t fifo_status;
 iis2iclx_fifo_status_get(&dev_ctx, &fifo_status);

 if (fifo_status.fifo_ovr_ia == 0) {
 /* Read magnetic field data */
 uint8_t fifo_data[112];
 iis2iclx_read_reg(&dev_ctx, IIS2ICLX_FIFO_DATA_OUT_TAG, fifo_data, sizeof(fifo_data));
 ...
 }
 ...
 }
 ...
}

This is my code, after INT1 triggers, it will sent a event, then read fifo_status2 and FIFO_DATA_OUT. 
Furthermore, I found that although INT1 was not triggered, but the fifo_data_level register was indeed increasing.