Skip to main content
NBerr.1
Associate
June 29, 2024
Question

IIS2DLPCTR ODR Accuracy

Could you please provide information about the output data rate (ODR) for the IIS2DLPCTR accelerometer?

For example, if I want an ODR of 50Hz in High Performance mode, with BW=ODR/2, how accurate is the 50Hz ODR?  Similarly, if I use the single data conversion on-demand mode at 50Hz, what would the accuracy be (assuming a perfect 50Hz trigger on INT2)?

 

Thanks.

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
July 4, 2024

Hi @NBerr.1 ,

From characterization measurements the ODR accuracy of IIS2DLPCTR is +/- 15%, note that it is tested on a limited number of samples and thus not guaranteed in production.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
NBerr.1
NBerr.1Author
Associate
July 4, 2024

Thanks Federica. When using ‘single data conversion on-demand mode’, how accurate is the actual sampling of the MEMS device relative to  the trigger signal on INT2?  In this case I’m not referring to T_on. I’m more interested in how ‘true’ the sample time is in this mode. In other words, if I  have a rising edge on INT2 to request a sample, how much internal delay will there be before the part’s internal ADC takes a sample?

 

 

 

NBerr.1
NBerr.1Author
Associate
July 5, 2024

For this, I am assuming the case where SLP_MODE_SEL = 0.