Skip to main content
apennell001
Associate
April 12, 2017
Question

IIS2DH Reading FIFO

Posted on April 13, 2017 at 01:08

With a 2g scale sampling @25Hz the FIFO fills with data and I am reading the contents up to the watermark. HR and LPen are disabled.

With the Z-Axis pointing toward earth I get the following data for the X-Axis using the H and L bytes:

DATX=128

DATX=128

DATX=128

DATX=-64

DATX=192

DATX=-128

DATX=-64

DATX=0

...

First, why are the values multiples of 32? Second, why the variability when the chip is still and not moving? I have been using the LIS3DSH for a couple years now so this IIS2DH is a real downgrade for sure, but I must be missing something. I have read over the manual several times now and can't find my issue. 

-AP

    This topic has been closed for replies.

    2 replies

    ST Employee
    April 13, 2017
    Posted on April 13, 2017 at 09:56

    The values are actually multiples of 64, because the FIFO contains 10-bits values. 10-bits value are left adjusted in output register which is 16 bits.

    You should divide the value by 64 and then multiply by the sensitivity.

    The variation is caused by the inherent noise. There could be also small vibration of the desk where the sensor is places.

    apennell001
    Associate
    April 13, 2017
    Posted on April 13, 2017 at 14:42

    Ahh, of course...I was treating it like a 16bit value. The variance in the values also make more sense now. Thanks for the quick reply!