Skip to main content
Associate II
Jul 7, 2025 7:16 AM UTC
Solved

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

The following text is quoted from 「Application Note "Qvar sensing" (AN5755) p2.

「 A signal is derived from the electronic circuit due to the fluctuations in the electric field resulting from the passage of the charged particles. If the electrode is embedded in an insulator or there is no direct contact between the electrode and the particles, the sensing process is achieved through electrostatic induction. 」



This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 7, 2025 1:10 PM UTC

Hi @Shion ,

When the electrode is embedded in an insulator, the sensing process at the electrode is primarily electrostatic induction, but it is strongly influenced by dielectric polarization of the surrounding insulator.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 7, 2025 1:10 PM UTC

Hi @Shion ,

When the electrode is embedded in an insulator, the sensing process at the electrode is primarily electrostatic induction, but it is strongly influenced by dielectric polarization of the surrounding insulator.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ShionAuthor
Associate II
Jul 8, 2025 12:13 AM UTC

Hi @Federica Bossi

Thank you for your comment. That being said, it was so. Is there a document that explains in detail the physical principles of this sensing? If so, I would appreciate it if you could let me know.