Skip to main content
AWool.1
Visitor II
March 2, 2022
Solved

I3g4250d temperature data invalid for 1 second (STM32F411VE-Disco)

I am writing a driver to retrieve data from the I3G4250D gyroscope embedded in the STM32F411VE discovery board (MB1115D). When the sensor starts up, the first 1 second of data contains an invalid temperature value (typically showing -7). After one second this value changes and is accurate from then on.

I noticed from the datasheet that there is a 1 Hz refresh rate for the temperature, which makes sense given what I'm seeing. I'm wondering if there's a way I can retrieve valid temperature data earlier than 1 second, i.e. if I can delay when this refresh rate begins. This temperature data is critical for our calibration calculations, so having bad data is messing up our algorithms.

This topic has been closed for replies.
TSand.1
TSand.1Best answer
Visitor II
March 4, 2022

Hi @AWool.1​ , you are right, the I3G4250D temperature sensor refresh rate is 1Hz, so you have to wait at least 1 second to get a correct readout of the temperature data. Unfortunately I don't believe there is a way to overcome this limitation, maybe you can try to read at least 1 second after the power up.

/tim

1 reply

TSand.1
TSand.1Best answer
Visitor II
March 4, 2022

Hi @AWool.1​ , you are right, the I3G4250D temperature sensor refresh rate is 1Hz, so you have to wait at least 1 second to get a correct readout of the temperature data. Unfortunately I don't believe there is a way to overcome this limitation, maybe you can try to read at least 1 second after the power up.

/tim